Industry Online Support
Technical Forum
8/13/2008 11:19 AM | |
Posts: 220 Rating: (14) |
Hi Nic_c, you can use RS232-Port via zero-modem-cable or ethernet. But just in case the MPI-interface is really damaged try the zero-modem for load the image and in the tab OS-Update there's beneth the path a checkbox, that one should be checked. The Imagetransfer may need very longer, but after that control the mpi-interface again. If it doesn't work after that you should exchange the panel. On this sites too Service and repairlinks where you can have look. first i suggest a transfer with resseting the panel, maybe that alone will help you. Zero-modem: http://support.automation.siemens.com/WW/view/de/21401061 regards Aranel |
Follow us on