1/14/2010 2:27 PM | |
Joined: 10/7/2005 Last visit: 9/23/2023 Posts: 2987 Rating:
|
Hello MITISH I presume by "SFC" for Step 7 you do actually mean S7 Graph (SFC is strictly speaking part of PCS7 and a bit more powerful than it's "poor cousin" S7 Graph) As for your questions:
absolutely, your S7 Graph sequence simply compiles into an FB which you call from your user program.
You sure can, part number for current version of S7 Graph V5.3 is: 6ES7 811-0CC06-0YA5 Last but not least, if you want to program Sequencers graphically in Step 7then S7 Graph is the way to do so in my humble opinion. There's is of course nothing "wrong" with S7 HiGraph and you could (ab)use it to program Sequencers. S7 HiGraph is however a graphical State Machine programming enviroment and as such lacks things such as simultaneous branches and not the right tool (in my humble opinion) to implementsequencers. Note too that S7 Graph is part of Step 7 Professional and as such more likely to be used (and known) by people (S7 HiGraph mustalways be bought seperately and I have yet to find a customer who actually has or uses it). I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on