7/1/2021 4:47 AM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33441 Rating: (4153)
|
The bit V0.0 is a part of the Byte VB0. Also a part of the Word VW0 and of the Double Word VD0. If write in V0.0 and at the same time in VW0, you have a overlapping. AttachmentLOGO! Bit, Byte, Word and DWord.pdf (245 Downloads) |
This contribution was helpful to2 thankful Users |
7/1/2021 2:39 PM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33441 Rating: (4153)
|
Do you mean something like in attachment? |
7/1/2021 3:08 PM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33441 Rating: (4153)
|
In attachment a example.
AttachmentFrom Modbus to LOGO!1 and from LOGO!1 to LOGO!2.zip (238 Downloads) |
Follow us on