10/11/2020 8:02 AM | |
Posts: 1 Rating: (0) |
Dear Experts, I am in a critical situation here. Our PCS 7 has two monitors for Engineering and Operators. The Operator WinCC can not come up to load the process interface. Alot of error messages. Initially, the SQL Server (WINCC) could not start but now, it does but still WINCC can not load. The recent error message is "Cannot open WinCC project - Project Manager for configured server is not running. Check the computer name of the server." Note: The computer name of the server is correct. I will so much appreciate who will help through this. I wish I can get started soonest. Time is not on my side. Thank you all for your usual efforts. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2020 05:55:28New subject after splitting |
|
10/12/2020 7:51 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2152)
|
Hello Chigozie, Which version of PCS7/WinCC do you use ? see the compatibility tool https://support.industry.siemens.com/kompatool/pages/main/index.jsf
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on