1/28/2009 9:00 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi SSDD, i don't think you need upgrade ALL system, lets me tell few: 1- usually new releases are compatible with old (because you have to replace them when broken) 2- usually you can use new releases in old SW (like ...1ex20... in PCS7 v6.1) but you have to configure previuos release in you HW configuration (p.e. ...1ex11...) 3- when you configure old release means you are not going to use new feature, but you HW works properly with what you configured. So, in your project, you have to configure 6gk7443-1ex11-0ex0 card in HW configuration hoe explained in this link http://support.automation.siemens.com/WW/view/en/31674579 Sorry for late answer, hope can help you Regards |