8/13/2020 7:49 PM | |
Joined: 12/28/2016 Last visit: 8/28/2024 Posts: 434 Rating: (45) |
سلام You must install Update 8.2 |
https://pnap.ir |
|
8/14/2020 9:53 AM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33647 Rating: (4182)
|
Then can you also at every time write: Update the firmware, if it is possible. |
8/14/2020 11:16 AM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33647 Rating: (4182)
|
Your LOGO! is the actually LOGO!8.2. In the device selection it is a LOGO!8.FS4. For this LOGO! you need at least LSC V8.1. To use all functions, you need at least V8.2. Better is upgrading to the actually LSC V8.2.1. If your LSC version is a full version, then can upgrade for free. LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) It's a 1,3 GB sized complete package. After the download start the setup as a administrator. |
This contribution was helpful to1 thankful Users |
8/14/2020 11:39 AM | |
Joined: 1/24/2020 Last visit: 2/16/2022 Posts: 3 Rating: (0) |
Well, the update allows me to connect and transfer my program! Thank you for your help! |
This contribution was helpful to1 thankful Users |
Follow us on