9/13/2023 8:10 AM | |
Joined: 1/20/2022 Last visit: 7/31/2024 Posts: 368 Rating: (3) |
hi All Can PLCSim communicate with real unified panel? This could be used for testing when PLC is not around. Regards |
9/13/2023 10:54 AM | |
Joined: 12/18/2014 Last visit: 8/4/2024 Posts: 33479 Rating: (4158) |
With the help of SIMATIC S7-PLCSIM Advanced virtual controllers for the simulation of a S7-1500 or ET 200SP CPU are created and used for the comprehensive simulation of functions. This means that no real controllers are required to test a STEP 7 program. Getting started with S7-PLCSIM Advanced and simulation tables |
This contribution was helpful to1 thankful Users |
Follow us on