11/6/2017 8:05 PM | |
Joined: 9/29/2014 Last visit: 8/6/2022 Posts: 60 Rating: (1) |
finally we change the winding field because the old was burned and now measure 351Vdc and 1.2 A in new winding field and 11Vdc and 1.2 A in armature field . my question is if I can reduce the current to my system without having a problem ; in the manual of my converter i read that there is a B+ potentiometer through which i can limit the current Can i regulate potentiometer B+ directly or I have to follow a specific procedure; Finally, someone knows if i adjust this potentiometer i only affect the current field or the armature field or both ; ------------------------------------------------------------------------------------------ |
Last edited by: Nikolaosst77 at: 11/7/2017 9:46:57 PMLast edited by: Jen_Moderator at: 11/8/2017 9:06:01 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
Follow us on