5/14/2019 10:46 AM | |
Joined: 12/8/2010 Last visit: 8/2/2022 Posts: 25 Rating: (2) |
Hello to everyone I have the same problem, just the OP is OP77A. I couldn't to communicate to the OP. I have two interface: 1- PC Adapter USB A2 (6GK1571-0BA00-0AA0) 2- Communication processor CP 5512 (6GK1551-2AA00) Can I communicate to the OP with these interfaces? If yes, what is my problem? Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/15/2019 09:58:02New subject after splitting Last edited by: Jen_Moderator at: 05/15/2019 09:58:23Optimized headline. |
|
5/15/2019 10:22 AM | |
Joined: 5/28/2008 Last visit: 6/8/2024 Posts: 4509 Rating: (837) |
Hello, There are more than one purpose of communication to SIMATIC HMI Panel.
In the attached excel sheet you can use filter feature and see what exactly cables / adapter you need for each communication purpose. Moreover for some panels, PC adapter can be used... The following section is extracted from this link:
Hope this helps Attachment19109408_wincc_flexible_projekttransfer_e.xlsx (93 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
5/19/2019 4:59 AM | |
Joined: 12/8/2010 Last visit: 8/2/2022 Posts: 25 Rating: (2) |
Hello Thanks for your answer. So, I should be replace it. Good Luck |
Follow us on