12/14/2021 2:13 PM | |
Posts: 12 Rating: (0) |
Hi, I have bought differtent logos which i will use as master/slave. I have one Logo 8 12/24 RCE as master and 2 logos 8 RCEo as slave. I want to connect the 3 modules with an CSM12/24 communication module. The problem now is that I can't connect my laptop with the 2 logos 8 RCEo because I think i can"t find the correct IP adress of them (this logos are without screen and I can not check the right Ip adres on my laptop). -> unable to finish the test correct. The slave module I can connect and download the program from my laptop to the logo. How can I get connected with my 2 slave modules, what is the IP adress of them?? Many thanks for your quick response. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/14/2021 15:07:45New subject after splitting |
|
12/14/2021 3:37 PM | |
Posts: 12 Rating: (0) |
Dear, Many thanks in advance. I see that 2 modules have the same IP adres. Will they be able to communicated with eachother? |
12/14/2021 4:15 PM | |
Posts: 12 Rating: (0) |
Dear, That's great but I am unable to change it. (see attachtment) If I change it in the white form, i am not able to connect. |
12/14/2021 4:32 PM | |
Joined: 12/18/2014 Last visit: 5/25/2024 Posts: 33106 Rating: (4087)
|
By me works it without problems, see attached screenvideo. Edit: Have you pressed the button "Assign IP address" if you have entered the new address? AttachmentChange IP address via LSC.zip (266 Downloads) |
Last edited by: ixo65 at: 12/14/2021 16:35:26 |
|
12/14/2021 4:44 PM | |
Joined: 12/18/2014 Last visit: 5/25/2024 Posts: 33106 Rating: (4087)
|
Which IP address and subnet mask have your Laptop? |
12/14/2021 5:15 PM | |
Posts: 12 Rating: (0) |
If i want to download program from laptop to slave. I have always the same window. I am getting to be lost... |
12/14/2021 5:18 PM | |
Posts: 12 Rating: (0) |
192.168.0.9 |
Follow us on