9/7/2011 4:28 PM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello, why do you "need" 19200? Have you allready try the other ones? Wich cable do you use? best regards |
9/8/2011 8:59 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
Hello, Read carefully this FAQ: http://support.automation.siemens.com/WW/view/en/23787153 Best regards, Hristo Mihalev |
9/9/2011 8:56 AM | |
Posts: 122 Rating: (1) |
Thank you for answers. UMENCHO I read tips. The problem is that I can't choose speed 19200 like is shown here https://a248.e.akamai.net/cache.automation.siemens.com/dnl/Tk2ODI3AAAA_23787153_FAQ/WinCC_flexible_Seriell_Transfer_10_e.gif Here is my configuration. One CPU214 comunicate through MPI with TP177Micro, communication speed is 19200, delay time in TP177Micro was configurated 0 and project starts immediatly - in this case I don't have acces to control panel of panel to change speed. Remote control is enabled. From TP177 manual: With the value "0", the project starts immediately. It is then no longer possible to call the loader after switching on the HMI device. In this case, an HMI device with the function "End project" would have to be configured. How to configure panel with "End project" function ? |
Follow us on