1/8/2014 6:04 AM | |
Posts: 515 Rating: (56) |
hi, do u mean that the accessible device(CPU) is not getting detected for the first time download? Try restart both your PC and plc and try again please.
|
1/11/2014 8:28 PM | |
Posts: 10 Rating: (0) |
Hi Randy I've tried all,but it not works.I can't conect and i can't start the plc.The RUN/STOP led it still blinking and remains yelow.And tia v 11 can't conect with this plc. It is CPU 1212C AC/DC/RLY and is a F.S 1 Fw 3.0.1 PLC.Order code 6ES7 212-1BE31-0XB0.I can not find this code in tia portal.The version of the software is Tia Portal Version V11 SP2 Update 2
Attachmentplc s7-1200.zip (449 Downloads) |
Last edited by: cristiandoom at: 1/11/2014 9:11 PMPlease helllpppppppp!!!!!!!!! Last edited by: cristiandoom at: 1/11/2014 9:08 PM |
|
1/11/2014 9:12 PM | |
Posts: 10 Rating: (0) |
best regards |
1/14/2014 6:15 AM | |
Posts: 10 Rating: (0) |
Thank you very much.I will do it and after that i hope it will work. Wish you all the best.
|
1/14/2014 8:48 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello cristiandoom, Here you can download latest update: Updates for STEP 7 V11 SP2 and WinCC V11 SP2 And the HSP: STEP 7 (TIA Portal) V11 Support Packages for the hardware catalog in the TIA Portal Best regards, Wizard |
1/15/2014 10:28 AM | |
Posts: 10 Rating: (0) |
Hi Wizard, I've reinstaled Tia Potall software and after that the updates but i can't instal HSP_11. Here are some pictures. What i'm dooing wrong? I don't understand why i can't install the HSP_11! Best regards.
Attachmentplc s7-1200.zip (366 Downloads) |
Follow us on