5/14/2019 9:17 PM | |
Joined: 6/1/2017 Last visit: 5/8/2024 Posts: 13 Rating: (0) |
Hi everyone I take a machine backup using simetic manager V5.5 sp4 .Problem is created when I find analog addresses PIW & PQW in cross reference but nothing to show and then I also open every FCs And FBs but also failed to find any PIW & PQW . Program is in STL Indirect pointer addressing and I am weak in pointer indirect addressing. please anyone open my attached program and go to HW configuration then see profibus adress 60 & 70 then see analog address and then find these addresses in program. pointers are mostly used FBs 80 to onward & FCs 80 to 89. Please I am in trouble help me as soon as .I take a project but nothing to understand . My final aim is to change analog addresses in HW config & in program . please check my attached program. THANKS ------------------------------------------------------------------------------------------ AttachmentRanatex_.zip (132 Downloads) |
Last edited by: Jen_Moderator at: 05/15/2019 06:35:10New subject after splitting |
|
5/15/2019 9:04 AM | |
Joined: 4/17/2018 Last visit: 6/4/2024 Posts: 262 Rating: (60) |
Hello Hafiz, In your program analog inputs are treated in FB50 and analog outputs in FB51 using indirect addressing. So which address you want to change? BR |
This contribution was helpful to1 thankful Users |
Follow us on