1/10/2012 8:49 AM | |
Joined: 10/10/2005 Last visit: 3/16/2023 Posts: 1909 Rating:
|
Hello, I think that the interface parameter are not correct in this case. There is a FAQ in the internet which descibe the steps which do you have to do if you load the moduls in the CPU. Please see the link: http://support.automation.siemens.com/WW/view/de/41885694 With best regards |
Follow us on