3/18/2019 2:31 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
I could not change the IP address. I just tried with 192.168.0.203 too? |
3/18/2019 2:44 PM | |
Joined: 2/22/2008 Last visit: 6/12/2024 Posts: 2698 Rating: (207) |
You also can use a little ip scanner, if you have problems to find a device. I often use this scanner Link See attached picture of a possible result of the scanner. Networks are not easy, if there is a little fault in the configuration. You need the right ip adrress, right subnet mask and pay attention, not to use an ip address a second time. These are only the main objects to mind. Regards, Scorp |
This contribution was helpful to1 thankful Users |
3/18/2019 2:48 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
Here is the screenshot with ipconfig /all. |
3/18/2019 3:15 PM | |
Joined: 12/18/2014 Last visit: 7/29/2024 Posts: 33437 Rating: (4153)
|
Can it be that a firewall is blocking the ports? Have you ever turned off the Firewall? |
3/18/2019 3:29 PM | |
Joined: 12/18/2014 Last visit: 7/29/2024 Posts: 33437 Rating: (4153)
|
Can you ping the LOGO! ? ping 192.168.0.3 |
Follow us on