7/25/2011 2:36 PM | |
Joined: 3/15/2008 Last visit: 5/28/2024 Posts: 106 Rating: (1) |
hi all, I have soft as I attached in csv file andI can't install update of PDM. During installation I get following message box: This product cannot be installed over the existing version of SIMATIC PDM K06.00.01.00. Setup will be closed. Does anyone know that I don't do correctly? or What did I in incorrect way? Iinstalled newES and I did following steps: - windows xp has been installed - sql server has been installed - PCS7 for ES has been installed. problem is only with the update of PDM. Thanks in advance AttachmentISS.zip (116 Downloads) |
Last edited by: irb6 at: 7/27/2011 8:02 AMSorry, the attached file is available now. Last edited by: irb6 at: 7/25/2011 2:36 PMBest regards |
|
7/26/2011 6:18 PM | |
Posts: 2661 Rating: (279)
|
Where is the "attached CSV" file? Also, please attach Citamis.str file found in C:\Windows and post a screenshot of the error message. Regards |
7/27/2011 8:10 AM | |
Joined: 3/15/2008 Last visit: 5/28/2024 Posts: 106 Rating: (1) |
Hi Phantom75, sorry for my mistake. Requested files have been attached in *.zip file. Regards AttachmentPDM_setup_error.zip (119 Downloads) |
Best regards |
|
7/29/2011 12:57 PM | |
Joined: 3/15/2008 Last visit: 5/28/2024 Posts: 106 Rating: (1) |
Hi Phantom75, your solution does not work in my case. I have uninstalled PDM and after that I could not install PDM mentioned in the topic. See the attachment. AttachmentSIMATIC PDM SETUP.zip (106 Downloads) |
Best regards |
|
7/29/2011 6:18 PM | |
Posts: 2661 Rating: (279)
|
Can you tell me what you uninstalled using the Control Panel? There are two components that have to be uninstalled. |
8/1/2011 7:58 AM | |
Joined: 3/15/2008 Last visit: 5/28/2024 Posts: 106 Rating: (1) |
Hi Phantom75 I have uninstalled PDM V6.0+SP1. Can you be less enigmatic and tell me what should I uninstall? :) Regards |
Best regards |
|
8/1/2011 11:53 PM | |
Posts: 2661 Rating: (279)
|
Hi irb6, You have to uninstall PDM Base & the PDM PCS7 Extension. See screenshot. Regards |
8/2/2011 8:02 AM | |
Joined: 3/15/2008 Last visit: 5/28/2024 Posts: 106 Rating: (1) |
Hi Phantom75, |
Best regards |
|
8/2/2011 5:48 PM | |
Posts: 2661 Rating: (279)
|
From the attachments I can see you have PCS7 V6.1 SP1 and you are trying to upgrade SIMATIC PDM from V6.0 SP1 to V6.0 SP2 HF1. But in any case it has nothing to do with the problem at hand. The only thing I can think of id there was a problem with your initial PDM installation. Please try to upgrade to SP5: SIMATIC PDM V6.0 + SP5 Released for Delivery |
8/3/2011 12:25 PM | |
Joined: 3/15/2008 Last visit: 5/28/2024 Posts: 106 Rating: (1) |
Hi Phantom75, I have installed PDM 6.0 SP5 succesfully. When I retrieve project that made with PDM 6.0 SP1 in new ES, in properties of project -> required software package next to PDM there is information: older version or not fully installed. If I saved multiproject with reorganization would it be correct and work as it in previous ES? Will project lost any information after reorganization? Regards |
Best regards |
|
8/3/2011 5:44 PM | |
Posts: 2661 Rating: (279)
|
Yes, I have seen this message before. Sometimes it disappears after just a save in the new version. |
Follow us on