3/10/2016 2:30 AM | |
Posts: 2 Rating: (0) |
I can'n open Tia Portal V13 SP1 UD7, When I run download update Automation. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/11/2016 1:47:49 PMNew subject after splitting |
|
3/10/2016 2:32 AM | |
Posts: 2 Rating: (0) |
Can you help me? please! |
3/11/2016 2:09 PM | |
Joined: 5/12/2006 Last visit: 6/4/2024 Posts: 22254 Rating: (2986)
|
Hi, @ Ankurgamit + @gabbar If you read the screen message from plccongnghecao in the second post then he have already installed Tia Portal V13 SP1 UPD7, so the Updatepackage for TIA (Include Step7 and WinCC) is running on the System! @plccongnghecao Can you provide the setup Logfiles for a analyze what happens during the Installation? If the Updater don't find the Update 7 again you can download the Installfiles here: https://support.industry.siemens.com/cs/ww/en/view/109311724
Christoph |
Last edited by: ChristophD at: 3/11/2016 2:10:51 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on