4/20/2016 2:39 PM | |
Posts: 24 Rating: (1) |
Hi i have a problem with SFC14 block in step 7.i can't read inputs from ET200M and the RET_VAL always shows error code=8092 but i know i enter the correct addresses for all SCF14's pin LADDR=w#16#0 RET_VAL= MW10 RECORD=MW100 I appreciate if you tell me what should i do? thank you ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/20/2016 3:50:53 PMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
4/20/2016 2:52 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
What is the address of ET200 in H/W configuration? |
This contribution was helpful to1 thankful Users |
4/20/2016 3:02 PM | |
Posts: 24 Rating: (1) |
The address of ET200 in H/W config is 8187 the first card in ET200 is DI16*DC 24V=6ES7 321-7BH00-0AB0 and it's address is 0..1 |
4/20/2016 4:00 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
Could you attach your project H/W configuration here? |
Follow us on