2/17/2009 2:34 PM | |
Posts: 102 Rating: (9) |
Hi I haven't work with new versions of simatic net, but in the old ones it didn't work with PLC simulator. |
2/17/2009 2:48 PM | |
Posts: 327 Rating: (28) |
OK, thanks, that solves thefirst part. |
2/26/2009 2:52 PM | |
Posts: 327 Rating: (28) |
Sorry for the delay in replying. I've studied documentation more seriously this time, so I understand your questions about TSAP. I've also tried several things (different TSAP, unconfigured connection...) but none showed any progress. Also, I tried connecting to real CPU (the one I worked with in first place) and I couldn't get values even from it, although it worked before. But I think that was because of my experiments with TSAP. I've attached both projects so you can check it, one in this post and one in next one. "OPC" is same as the one I worked last week, minus DBs, FCs, additional hardware, etc. I've tried creating a simple SCADA with WinCC flexible and it works normally when connected to PC with WinAC. AttachmentOpc.zip (163 Downloads) |
2/26/2009 2:54 PM | |
Posts: 327 Rating: (28) |
Project for PC with WinAC Best regards, Filip Belic AttachmentWinac2.zip (144 Downloads) |
Follow us on