2/5/2017 1:51 PM | |
Posts: 10 Rating: (0) |
i would like to add new ET200M . i download gsd file form below link https://support.industry.siemens.com/cs/document/113498/profibus-gsd-files-%3A-et-200m?dti=0&lc=en-WW DESCRIPTION: Station type:ET 200M (IM153-2 High Feature) DPV1, H, 12 I/O and instal et200m gsd file but i cant see IM 153-2 module in the ET200M. Could you help me for this issue ? ------------------------------------------------------------------------------------------ |
Last edited by: Emil_Agasenov at: 2/5/2017 1:52:19 PMLast edited by: Min_Moderator at: 2/6/2017 3:57:58 PMNew subject after splitting |
|
2/13/2017 10:19 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Emil, Take the ET200M from HW-Catalogue in PROFIBUS-DP ->ET200M-> IM153-2 with correct MLFB Then you will see the IM153-2 in slot 2 If the IM153-2 is not in the HW-cataloge, try to install the latest Hardware Support Package or the latest SP for Step7 5.5. Service Pack 4 for STEP 7 V5.5 and STEP 7 Professional 2010 hope this helps, regards, |
FCK WAR! |
|
2/28/2017 7:32 PM | |
Posts: 10 Rating: (0) |
THANKS A LOT) VERY HELPFUL |
Follow us on