7/14/2020 8:23 AM | |
Posts: 11 Rating: (0) |
Hi all I have the same problem, I have a new S7-1200 PLC and I can't see to assign an IP. I already checked the service: PnDiscovery Service and it is running. Something else i can try? Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2020 11:20:19New subject after splitting |
|
7/14/2020 3:26 PM | |
Joined: 9/6/2015 Last visit: 9/7/2024 Posts: 141 Rating: (9) |
Can you use ping test to check reachability the target device using windows CMD? |
7/14/2020 3:31 PM | |
Joined: 7/7/2010 Last visit: 10/15/2024 Posts: 15316 Rating: (2431)
|
You are using V13? What operating system? V16 is the current version which is supports windows 10. V13, not so much (windows 10 anyway). Can you post a screenshot of the way you are trying to assign the IP address. Has it ever worked before?
|
science guy |
|
7/14/2020 3:57 PM | |
Posts: 11 Rating: (0) |
not because I don't know what the IP address is, it is a new S7-1200 PLC. According to the manual, the PLC has no IP address, only MAC address. Regards
|
7/14/2020 9:10 PM | |
Posts: 11 Rating: (0) |
Hello, first of all, thank you very much. Yes, I use Vercion 13. My operating system is window 10 Pro, 64 bits. Additional Information: I use a virtual machine. It is a new PLC7-1200 and I want to load a program (I already have the file). I don't know which fixed IP address I can put on my PC. Regards
|
7/14/2020 10:44 PM | |
Joined: 7/7/2010 Last visit: 10/15/2024 Posts: 15316 Rating: (2431)
|
Are you able to ping _any_ device from that VM? VMs can be tricky to get setup with networking.
|
science guy |
|
Follow us on