4/28/2020 2:05 PM | |
Posts: 75 Rating:
|
Dear experts, I have problem with MICROMASTER Integrated 6SE9612-7DF60ZC87.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/29/2020 06:12:59New subject after splitting |
|
4/29/2020 10:17 AM | |
Joined: 3/27/2008 Last visit: 7/18/2024 Posts: 1125 Rating:
|
The parts: PC connecting cable = 6SE3290-0XX87-8SK0, this is on RS Components, and appears to have the 'edge' connector for the RS 232 connection. https://uk.rs-online.com/web/p/miscellaneous/3214993/ Connector,cable,PC,MicroMaster invertor
I now see it is a discontinued item, but the information sheets and the picture of parts may be may be useful? Keypad OPM2 = 6SE3290-0XX87-8BF0, I see some on E Bay for sale, silly prices though. Comment: I would guess the parameters required for the pump to work with a new inverter brick will be small, and for simplicity, if you can get the OPM2 to function I would recommend commissioning the unit from default settings. I have some hard copy notes here if you need further information. Tractor |
Last edited by: Tractor at: 04/29/2020 10:18:42Last edited by: Tractor at: 04/29/2020 10:24:20Tractor |
|
4/29/2020 2:02 PM | |
Joined: 3/27/2008 Last visit: 7/18/2024 Posts: 1125 Rating:
|
Regarding software: STARTER does not do Combimaster / Micromaster Integrated Drive monitor should work with this drive, but I have not tried this for some time https://support.industry.siemens.com/cs/ww/en/view/11769381 The easiest route I believe is to make a cable to go between SK200 and the OPM2. SK200 DType 1 - +5v ----- 6 2 - n (-) ----- 8 3 - 0V ----- 4 4 - P (+) ----- 3 |
Last edited by: Jen_Moderator at: 04/30/2020 07:14:11Optimized link. Tractor |
|
Follow us on