11/11/2021 5:52 AM | |
Joined: 5/20/2019 Last visit: 4/16/2024 Posts: 4 Rating: (0) |
Dear Sir 1. Please advice whether the existing U23 with range in ppm can change becomes mg/m3 ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_7336015 at: 11/11/2021 05:59:01Last edited by: Jen_Moderator at: 11/11/2021 11:34:39New subject after splitting |
|
12/20/2021 8:28 AM | |
Joined: 11/20/2007 Last visit: 6/16/2023 Posts: 25 Rating: (3)
|
Yes, it is possible to change unit from ppm to mg/m3. First you have to change from ppm to vpm and then to mg/m3. |
1/11/2022 1:34 PM | |
Joined: 11/20/2007 Last visit: 6/16/2023 Posts: 25 Rating: (3)
|
You can change the units directly in the U23 menu. see attachment. If the units is shown in vpm, you can directly change to mg/m3. AttachmentU23 Unit change.docx (621 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on