11/30/2016 6:46 PM | |
Posts: 3 Rating:
|
Can the old Milltronics Hand Held Programmer be used for the earlier versions of Multiranger 200? we have for instance a SN PBD/E2140007 Multiranger 7ML50332AA102A in our mill stores I cannot find a part number for the old magnetic mount IR programmers, added as an accessory during ordering a Multiranger Plus in the old days, maybe 10A4-131, maybe now a 7ML58302AH, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/1/2016 1:17:13 PMNew subject after splitting |
|
12/6/2016 11:58 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating:
|
That´s right , only the overlay is different. Please note, that the handheld of the Multiranger has been changed to a new version. The version with the ordercode 7ML1830-2AK has beed replaced to the new compact version A5E36563512. Please fond also the attachment. Hope this helps ! AttachmentProgrammer overlay reference_with comments_CPU_corr.pdf (322 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on