2/28/2018 8:02 AM | |
Joined: 5/20/2015 Last visit: 9/11/2023 Posts: 210 Rating:
|
Dear all experts, i have 6ES7153-2AR04-0XA0 ET200M, IM153-2 INTERFACE REDUND.BUNDLE, it contains IM153-2 HF (6ES7153-2BA10-0XB0) AND Bus module for ET 200M for holding 2 IM153-2 red. (6ES7195-7HD10-0XA0). but in actual physical hardware integration IM153-2 HF is mounted on 6ES7195-7HB00-0XA0 (Bus module for ET 200M for holding two 40 mm wide I/O modules for removal and insertion function). will it works, i am getting bus fault on both bus BF1 and BF2. can we use 6ES7195-7HB00-0XA0 for connecting both whole rack of ET200M, IM153-2 INTERFACE REDUND.BUNDLE.with i/o modules help me ASAP. thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/28/2018 1:35:33 PMNew subject after splitting Let's do it... |
|
3/13/2018 1:49 PM | |
Joined: 6/19/2017 Last visit: 9/29/2023 Posts: 7350 Rating:
|
New question published by charlie87 is split to a separate thread with the subject CPU just stooped with no error announcment. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on