1/31/2019 8:32 AM | |
Posts: 21 Rating:
|
Hello, thing that makes me wonder, its the situation when we move axis from one position to other position with CommandTable. For example, after homing, and with conditions on CommandTable execute input, we want to move axis from 0 to 4500mm, where the other sensor awaits. Axis starts to move, but due to some noises it may loose steps/position and will not reach the sensor (but will reach position 4500mm anyway, but before sensor or after). Is there some method to prevent this? Can we use HSC on one of the inputs, and connect PTO output signal to HSC input and measure it somehow to make precise position? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/31/2019 12:45:35 PMNew subject after splitting Last edited by: Grzesiuk93 at: 1/31/2019 1:23:55 PM |
|
2/26/2019 4:26 PM | |
Joined: 4/28/2015 Last visit: 4/7/2025 Posts: 398 Rating:
|
Hello, is your motor loosing step because of overload...? |
This contribution was helpful to
1 thankful Users |
Follow us on