3/8/2023 11:19 PM | |
Joined: 2/25/2023 Last visit: 10/22/2023 Posts: 5 Rating: (0) |
Can we use the set/reset flip flop in fbd to make a sigle button On/Off switch? Like on set we connect a Hmi button to set the output on the first press then on Reset we make AND connect the same set button and the Output variable? So on the second button press it would check that Output is on and reset the Set/Reset flipflop. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/09/2023 09:39:41New subject after splitting |
|
3/13/2023 10:36 AM | |
Joined: 2/25/2023 Last visit: 10/22/2023 Posts: 5 Rating: (0) |
I did the same but it doesn't reset, Can you check what I have done fell? I am new so. |
Follow us on