5/4/2023 9:04 AM | |
Joined: 12/25/2020 Last visit: 8/21/2024 Posts: 17 Rating: (0) |
dear all, Can we use V90 drive for encoderless operation or not ? Because when I am trying to use it for a encoderless motor it is showing fault 52983 :- encoder not detected. And i search for all the modes in V-assistant and there is no mode showing for encoderless operation. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/04/2023 12:17:26New subject after splitting |
|
5/4/2023 9:28 AM | |
Joined: 5/12/2006 Last visit: 10/8/2024 Posts: 22399 Rating: (3017)
|
no not supported |
This contribution was helpful to1 thankful Users |
5/8/2023 6:32 AM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (1) |
Hi gsfouzdar, Not possible. Choose incremental or absolute encoder for precious measuring. Do share your complete application details.
|
If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
This contribution was helpful to1 thankful Users |
Follow us on