3/10/2009 9:15 AM | |||||||||||||||||||||||||||||
Posts: 6 Rating:
|
I couldn't solve exactly how 3rd degree POLY command works, i will be very glad if you help me to write only 1 line from this data set. The values are also available in excel format in the attachments. C axis is the rotary axis around Z axis, and V is the same as X. It is also in the attachment. Thanks,
Attachmentcam.zip (283 Downloads) |
||||||||||||||||||||||||||||
Last edited by: Ruselgun at: 3/10/2009 7:21 PM |
|||||||||||||||||||||||||||||
Follow us on