4/3/2013 12:45 PM | |
Joined: 4/22/2010 Last visit: 10/17/2024 Posts: 5697 Rating: (715)
|
Hello Battery should be replaced with power on, run or stop does not matter. Before you change a buffer battery you have to depassivate it. Proceed as follows: 1. Set the switch Batt Indic to Off. 2. Remove the old battery/ batteries. 3. Depassivate the new battery/ batteries by short circuiting the poles for 1 to 3 seconds. 4. Insert the new battery/ batteries. 5. Set the switch Batt Indic to 1 Batt or 2 Batt. For depassivation see: Why is a battery fault signaled when you insert a back-up battery, even though the battery is new? Regards, Marcjan |
Problem solved? |
|
4/4/2013 9:21 AM | |
Joined: 11/17/2011 Last visit: 6/17/2024 Posts: 123 Rating: (1) |
thanks you very much, |
Follow us on