4/12/2020 9:08 AM | |
Posts: 1 Rating: (0) |
Hello everyone, I am new to PLC programming and just bought my new S7-1200 Starter Kit. My controller is AC/DC/RLY. ISSUE: I can configure my controller after creating/opening a project since I know the exact type of my controller. However, when I go to the next step, where I need to download my program to my PLC. I cannot connect to my PC. I have attached the screenshot of the window that pops up when I try to download my program to my device. I also tried to select the Profinet option here along with my Realtek controller. and have tried the use the same IP address as that of the controller (192.168.0.1) except for the last entry (i.e 192.168.0.2). but in vain. I would appreciate it if anyone can point out my mistakes. Thank you very much in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/13/2020 11:07:26New subject after splitting |
|
4/12/2020 9:34 AM | |
Joined: 2/5/2013 Last visit: 10/6/2024 Posts: 321 Rating: (74) |
Hi AutoGen_2695267, Attached Manual will be helpful to you. If you are beginner and want to learn the please visit this Link Br, AmolG. Attachment1200.pdf (46 Downloads) |
Last edited by: AmolG at: 04/12/2020 09:42:16Please rate it. |
|
Follow us on