2/23/2023 8:24 PM | |
Joined: 6/24/2021 Last visit: 5/16/2023 Posts: 2 Rating: (0) |
Did anyone ever solve the problem of why the CPU needed to stop? I have a CPU now that I cannot download even a small change without the CPU having to stop. This CPU did not require stopping untill recently. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/24/2023 05:04:26New subject after splitting |
|
2/24/2023 6:11 AM | |
Joined: 3/11/2019 Last visit: 5/8/2024 Posts: 1408 Rating: (255) |
Hi logix2013, with this amount of detail, we could not really help you. In general there are some preconditions for download in RUN mode. With following link you can find a table, for different CPU base models and which actions are needed or possible to download in RUN. Downloading blocks in the "RUN" operating mode to the device-> if you scroll down in this link, the table mentioned could be found regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on