4/15/2016 9:43 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:51:58 AM~(‾▿‾)~ |
|
4/15/2016 10:12 AM | |
Joined: 4/22/2010 Last visit: 6/5/2024 Posts: 82 Rating: (1) |
My main problem is that the ES cant see if the master was activated or not. |
4/15/2016 10:15 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:52:07 AM~(‾▿‾)~ |
|
4/15/2016 1:16 PM | |
Joined: 3/14/2008 Last visit: 6/6/2024 Posts: 2070 Rating: (928) |
You can check the following FAQ. Delta Loading OS Are all users and passwords the same on ES, OS servers? Are they all member of "SIMATIC HMI"? Did you set the "terminal bus" to the first position in Simatic Shell? Is the redundancy configured correctly in Simatic Shell? Did you set: "Default Master" in the WinCC explorer->Redundancy settings? Please make sure that the master server has this option only..not both! Did you reposition the project on another directory? Please run SimaticRights.exe program in order to restore those settings.. |
Last edited by: Oreca at: 4/15/2016 1:19:35 PMIf I could help you, you can use the RATE button. Thank you. |
|
4/19/2016 7:45 AM | |
Joined: 3/14/2008 Last visit: 6/6/2024 Posts: 2070 Rating: (928) |
Goodmorning! Uhm, maybe a few things worth to check out. Are you logged in to your ES with the new username? or did you also tried with the old username to download changes? And you created a new username or did you change the old name to the new name. I hope not, because that can give you trouble... Do you have full read and write access to the shared folders of the OS project on the servers with your new username? (also simple file sharing deactivated) Maybe this FAQ can help you: Download change Can you see both servers in Simatic Shell? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on