8/11/2020 12:18 PM | |
Joined: 5/24/2018 Last visit: 2/7/2023 Posts: 26 Rating:
|
Hello , But in the case of having a dp / pa collector how would it proceed, according to what I found is through a gsdtool tool and here include the gsd file of the profibus pa instrument, the detail is that I do not know how to configure the data types in the gsd and I give it everything by default, as I am working with the im153-2 it would be a dp / pa link, when I already load the gsd I follow the steps and I put address 2 to the coupler both in hardawre siemens and softawre abb, I would have to put an address to the instrument pa ?? And if this is how I would declare it in abb, since I cannot establish communication, I remain attentive to the comments ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/11/2020 12:48:44New subject after splitting |
|
8/13/2020 5:12 AM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33450 Rating:
|
Please write in english... |
8/13/2020 5:20 AM | |
Joined: 5/24/2018 Last visit: 2/7/2023 Posts: 26 Rating:
|
I already corrected it . Thank you |
This contribution was helpful to
1 thankful Users |
8/13/2020 2:49 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating:
|
Hello Hernan; First, is this the document you have been consulting to configure your DP/PA Link on your ABB Profibus-DP master? How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5? (GSD tool) https://support.industry.siemens.com/cs/ww/en/view/26562190 From the contents of your post, it seems you have followed the steps pretty well. But your screenshot shows diagnostic messages on your ABB hardware (AC 800M and CI854, it seems), can you investigate what the ABB CPU is complaining about? A BF signal shows detection of a bus fault, generally a discrepancy between the address of the Profibus node and the configured address in the master's configuration software. Does the BF appear on the IM 153-2 or on the FDC 157-0? Check the information available in the DP/PA link manual you can download from the GSD tool link above: Address (Profibus-DP) of the IM 153-2 :(check the addressing diagram, it is often a source of problems, the LSB of the dipwitches is not used for addressing. For Profibus address 2, only diswitch #3 should be on.). https://support.industry.siemens.com/cs/ww/en/view/1142696/29932665483 LED displays on the DP/PA coupler (part of the DP/PA link: https://support.industry.siemens.com/cs/ww/en/view/1142696/29934856971 Our projects team has used the DP/PA Link and Simatic PDM with Controllogix (Rockwell) and RX3i (GE) CPUs in the past, and I can assure you that if the gsd file is properly setup and the hardware configured adequately (no BF!) it transfers the instrumentation data quite reliably. Concentrate on the BF LED, this seems to be the error message that is blocking you; when you correct the issue you should see data exchanges on the DP/PA link. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/13/2020 15:15:31Last edited by: dchartier at: 08/13/2020 20:14:31 |
|
This contribution was helpful to
1 thankful Users |
8/14/2020 5:54 AM | |
Joined: 5/24/2018 Last visit: 2/7/2023 Posts: 26 Rating:
|
|
8/14/2020 5:59 AM | |
Joined: 5/24/2018 Last visit: 2/7/2023 Posts: 26 Rating:
|
|
Follow us on