5/27/2019 8:28 AM | |
Joined: 3/10/2016 Last visit: 5/28/2024 Posts: 14 Rating:
|
Hello dears, I met a problem on TP1200 panel runtime page, in TIA V14 SP1, i called OpenInternetExploron on a button, this call a website which display Siemens camera image, on TP1200, when i click this button, the website can display fully with image, then i click CLOSE symbol on Internet menu, it is strange that the top of this InternetExplorer cannot disppear, and it seems dead, no any feedback while i click the internet memus, but when i click OpenInternetExplorer button again, the website appear fully again, but same dead while i push Close button on Internet software. I donot know why it like this, on control panel---Internet options, inside i can adjust cached size, now it is 512Kb, if i make this larger, can solve this issue or not? Thanks in advance AttachmentPictures.zip (37 Downloads) |
Last edited by: Jen_Moderator at: 05/27/2019 14:17:38Added all pictures as an attachment. |
|
Follow us on