3/12/2021 5:17 AM | |
Joined: 9/26/2012 Last visit: 6/6/2024 Posts: 4 Rating: (0) |
Goodnight, I have a 6es7512-1sk01-0ab0 cpu that is in version V2.0.3 of firmware in version V13.0 SP1 TIA, the problem is that I cannot find this version in my TIA 13 catalog, thank you. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/12/2021 08:57:03New subject after splitting |
|
3/12/2021 12:10 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi LuisAraujo, go to Online&Diagnostics. You can find the project-version which is loaded to the PLC. When the versions are different, there is a FAQ, that explains what to do: What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?hope this helps, regards, |
FCK WAR! |
|
3/12/2021 12:33 PM | |
Joined: 9/26/2012 Last visit: 6/6/2024 Posts: 4 Rating: (0) |
OK friend, when I checked online (I no longer have the photo) it showed me a message that the cpu off line v1.8 was not compatible with the online version 2.0.3, even though the CPUs are the same, except for the firmware. In TIA portao V13 SP1 |
Last edited by: LuisAraujo at: 03/12/2021 12:34:43 |
|
Follow us on