Industry Online Support
Technical Forum
5/17/2013 8:13 AM | |
Joined: 5/12/2006 Last visit: 1/17/2025 Posts: 22497 Rating: (3044)
|
Hello, which Operation System and which Step7 Version do you use? Regards Christoph |
5/17/2013 8:17 AM | |
Joined: 1/6/2011 Last visit: 8/29/2024 Posts: 45 Rating: (0) |
WIN XP SP3 STEP 7 V5.5 |
5/17/2013 2:22 PM | |
Joined: 1/6/2011 Last visit: 8/29/2024 Posts: 45 Rating: (0) |
can you tell me where can find the driver files to re-install. I didnot find it anywhere ? |
10/16/2013 11:04 AM | |
Posts: 5 Rating: (0) |
I had uninstalled & installed the Drive starter & step7 V 5.5 but still the usb 7 option is not displaying in pg PC interface |
10/16/2013 12:06 PM | |
Joined: 5/12/2006 Last visit: 1/17/2025 Posts: 22497 Rating: (3044)
|
Hello, which OS do you use? Have you install first Step7 and then starter? Regards Christoph |
Follow us on