2/23/2018 10:07 AM | |
Joined: 1/24/2015 Last visit: 10/27/2021 Posts: 193 Rating: (7) |
Dear All; It is ok to activate PID Block. But in my PID block there is no ModeActivate so I cannot find the modeactivate binary in PID DB. What is the way to obtain this button. Best Regards... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/23/2018 1:48:17 PMNew subject after splitting |
|
2/23/2018 3:53 PM | |
Joined: 7/7/2010 Last visit: 6/3/2024 Posts: 14755 Rating: (2377)
|
What PID block are you using, what PLC, and what Portal Version/ SP / update?
|
science guy |
|
2/23/2018 8:39 PM | |
Joined: 1/24/2015 Last visit: 10/27/2021 Posts: 193 Rating: (7) |
|
2/23/2018 10:23 PM | |
Joined: 7/7/2010 Last visit: 6/3/2024 Posts: 14755 Rating: (2377)
|
I opened a s7-1200 project, add new block -> FB, named it PID_Controls of type SCL I dragged in PID_3Step instruction to the block. Told it multi-instance so it created a static tag in the FB's interface. In that tag, the enable input is: PID_3Step_1.ModeActivate, an input to the PID instruction block. Is that what you were looking for?
|
science guy |
|
2/25/2018 8:00 PM | |
Joined: 1/24/2015 Last visit: 10/27/2021 Posts: 193 Rating: (7) |
Here the other function... Modeactivate bit is here.... |
Last edited by: Mert Turgut at: 2/25/2018 8:00:30 PM |
|
2/26/2018 8:13 AM | |
Joined: 3/19/2015 Last visit: 5/15/2024 Posts: 89 Rating: (27) |
Hi, is it possible that you use two different versions of PID_3Step? ModeActivate is only available with version 2.x of PID_3Step that is supported by 1200 CPUs with FW V4.0 or higher. 1200 CPUs with FW V3 or V2.x only support PID_3Step V1.x that has no ModeActivate. See https://support.industry.siemens.com/cs/ww/en/view/108210036/82198803595 for details regarding the versions. If you have a version V4.x of 1200 CPU you can switch from PID_3Step V1.x to PID_3Step V2.x by changing the library version e.g. in instruction task card of a programming editor. Regards |
This contribution was helpful to1 thankful Users |
2/26/2018 11:57 AM | |
Joined: 1/24/2015 Last visit: 10/27/2021 Posts: 193 Rating: (7) |
Yes, it may be. I will check it. Thank you. |
Last edited by: Mert Turgut at: 2/26/2018 5:49:10 PM |
|
Follow us on