2/8/2012 10:17 AM | |
Posts: 3037 Rating: (192)
|
Hello, Can you make a screenshot of this error message? Does the error message appear at all projects? Which version of WinCC V11 do you use? The newest version is WinCC V11 SP2. You can delete the folder "IM" in your project folder. Now you generate the project new. Have you WinCC V11 and WinCC V7 on the same computer? You should see the following link " which sofware of simatic work fine with WinCC V11". With what is SIMATIC WinCC V11 compatible? Tweety |
This contribution was helpful to1 thankful Users |
2/9/2012 1:21 PM | |
Posts: 3037 Rating: (192)
|
Hello, You see in the other folders under "General" if you find a place which is marked red. Can you find this place? If you do not find a place which marked red, then you can contact the customer support for behaviour. ----> customer support Tweety |
5/17/2012 3:33 PM | |
Posts: 54 Rating: (1) |
Hello, Same problem onmy pc. switch off AV mean? thanks |
8/15/2012 1:22 PM | |
Posts: 3037 Rating: (192)
|
Do you have this problem at all projects? Tweety |
8/15/2012 1:28 PM | |
Posts: 19 Rating: (0) |
only WinCC RT Professional Emerson
|
8/15/2012 4:06 PM | |
Posts: 3037 Rating: (192)
|
Has your administrator local administrator rights? Tweety |
8/15/2012 8:07 PM | |
Posts: 19 Rating: (0) |
my user is administrator Emerson
|
2/18/2013 10:49 PM | |
Posts: 5 Rating: (0) |
I solved it by using the "repair" with the installation setup of wincc package |
This contribution was helpful to2 thankful Users |
3/31/2013 6:30 PM | |
Posts: 9 Rating: (0) |
Hi, disabling two of the WINCC SQL Server services worked for me. See the attachment. Br, Igor
|
This contribution was helpful to2 thankful Users |
4/9/2014 9:30 AM | |
Posts: 2 Rating: (0) |
Hi; Problem solved. change your computer name. dont use special characters like - _ . ,
|
3/12/2021 4:47 PM | |
Posts: 11 Rating: (0) |
Hello I had a similar problem. It did not allow me to save the file or compile. To solve it disable my antivirus. |