9/10/2018 12:53 PM | |
Posts: 47 Rating: (1) |
Dear all experts, I've followed the instructions as attachment. I finished writing image file to microSD card without errors, then I plugged it to IOT module and powered on. The SD LED was flashing some times and turned off. The ethernet card of my laptop was set to 192.168.200.10 and I connected ethernet cable to X1P1 of IOT2040. The problem is I cannot ping to 192.168.200.1, so I cannot access my module by using Putty (it said network error). I've try some tips on the internet but it doesn't work. Please help me to solve this problem. Thank for your attention. AttachmentSIMATIC_IOT2000_Setting_up_V2.1.1.pdf (133 Downloads) |
9/10/2018 5:15 PM | |
Posts: 47 Rating: (1) |
Hi bergmanu, Thank you for your quick reply. I follow your instructions but nothing changes. I also use another SDcard, but it doesn't work. |
9/10/2018 6:38 PM | |
Posts: 47 Rating: (1) |
Hi bergmanu, https://support.industry.siemens.com/cs/ww/en/view/109745562 By the way, could you show me how the SD card's function in MindConnect IOT2040? I'm looking forward to hearing from you soon, and once again, sorry for my mistake. |
Last edited by: minhkhanh at: 9/10/2018 6:39:36 PMLast edited by: Jen_Moderator at: 9/11/2018 7:58:32 AMOptimized link. |
|
9/11/2018 8:43 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, did you use the µSD card which was included in the MindConnect IoT2040? If yes, I do not know if it is possible to restore the MindConnect IoT2040 image.. Please visit the MindSphere forum, maybe they can help you. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
9/11/2018 8:50 AM | |
Posts: 47 Rating: (1) |
Yes, I've used its own microSD card. :( It is an awful experience. I hope someone will help me to solve this problem |
Follow us on