10/31/2017 4:31 PM | |
Joined: 3/2/2015 Last visit: 10/8/2024 Posts: 45 Rating: (0) |
Hi SINAMICS experts :) I have a problem using STARTER V4.4.0.3 to program a SINAMICS non-programmed DRIVE-CLiQ encoder fitted to a 1FT7105-5AB71-1BH1 SINAMICS motor. I have a good 1FT7105-5AB71-1BH1 motor with good electronic rating plate data and another 1FT7105-5AB71-1BH1 motor with a new non-programmed encoder to be programmed with the data from the good one. The new encoder is brand new from SIEMENS authorised supplier. Type: 6FX2001-5JD24-2DC0. In the SIEMENS Encoder replacement in 1FK7 G2 and 1FT7 manual here, on page 41 it says How to save the electronic rating plate for a motor. It states: 1. Switch on the machine. My problem is thatI cannot find Parameters p4690 and p4691 anywhere in STARTER, not even in the help menu. I have Expert access enabled and p4690 and p4691 are not listed there. I have also downloaded the Electronic Rating Plate dqixe1.bin file from the DRIVE-CLiQ Data Download Services site using the serial number from the non-programmed motor. I attempted to program the encoder using this file but ran up against the same problem of not being able to access p4690 and p4691. From page 40.. To transfer the data to the encoder module Can anybody shed some light on this? Kind regards, Matt. |
11/1/2017 7:07 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (40) |
hello, Although you didn't advertise some details such as exact Drive type and so forth, I'll try to shed some light, so to speak, on the dark side of the moon...
P.S. For the reliability of our moon program please find screen shot attached. Msorich Attachmentp4690_location.pdf (399 Downloads) |
11/1/2017 9:53 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (40) |
have a fun! |
10/9/2019 1:11 PM | |
Joined: 8/21/2014 Last visit: 11/6/2024 Posts: 1024 Rating: (14) |
New question published by Vinicio Gomes is split to a separate thread with the subject Problems with parameter p4690. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on