11/2/2016 11:38 AM | |
Joined: 10/2/2015 Last visit: 8/8/2024 Posts: 9 Rating: (1) |
Hi... I am facing same problem... I am using TIA sp1 udp 9 .... while adding device proxy for simotion backup .. in setting Ethernet IP address disapear and not able to set... But If I am Open same simotion backup in TIA sp1 Upd 3 using device proxy, It allows and appears the ethernet addresses. Please help me to out this situation... ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/2/2016 4:27:07 PMNew subject after splitting |
|
11/15/2016 5:35 AM | |
Posts: 18 Rating: (0) |
I don't use the same products as you do, but maybe this can help, all the same: Have you considering trying to set the IP address using Siemens' Primary Setup Tool? It works for some things. Before I figured out to how to set IP addresses via the TIAP interface, I used it a fair bit. |
Follow us on