3/8/2013 11:03 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
1. In order to insert a Profibus slave must select Profibus line in hardware configuration. 2. There is not possible in case of 200S to insert modules without to have power modules between a few modules (how many modules it depends - this is other other story). 3. In attachment a saple project with both modules. Try it (using copy and paste). Best regards, Hristo Mihalev
AttachmentSample.zip (167 Downloads) |
3/8/2013 11:58 AM | |
Posts: 51 Rating:
|
I can also create a new IM151 on the profibus line and insert my two new cards, but my problem is that I cant do it on my existing IM151, that I think is from a GSD file ant not from the standard HW. I opened your project and also inserted the IM151 that is used on my project. Please test it and try to insert a 6ES7134-4MB02-0AB0 on that node. It probably wont work... The project already have 42 cards and nowIm about to change one of them and also add three more cards. I hope the hardware constructors know what they are doing regarding the power modules... AttachmentD:\tmp\upload\Sample2.zip (214 Downloads) |
Last edited by: CS Moderator at: 3/10/2013 6:50 PMAttachment reattached |
|
3/8/2013 12:10 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Correct! Let's check it there.
|
3/8/2013 1:51 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
I am not sure if you will have possibility to insert more then 244 bytes in 1AA03. Check it there -http://support.automation.siemens.com/WW/view/en/21406019 |
3/8/2013 2:15 PM | |
Posts: 51 Rating:
|
But I only have about 95 bytes or am I counting wrong? 4 bytes för each 2AI or 2AO and 1 byte för the others. |
3/8/2013 2:25 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
|
3/13/2013 7:25 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
In your project in Simatic Manager is possible to configure 6ES7134-4JB50-0AB0 and later on todownload to CPU. Phisically in 200S rack you can mount4JB51 without to change the hardware configuration and it will work. Just there have a limitations. You can not use the newer features of 4JB51.http://support.automation.siemens.com/WW/view/en/31713242
|
Follow us on