12/14/2023 2:14 PM | |
Joined: 12/10/2011 Last visit: 7/10/2024 Posts: 39 Rating:
|
This post is relative old, but I tried to retrieve it because is strictly correlated. I'd like to know what are the reasons that I cannot set a send clock less than 1ms? Because I have a 1517 3PN/DP with 2 modules connected to it, one 32DI e one 32DO and I have connected to PN a IM 155-6 PN HS with a 8DI HS. I set the isochronous parameters and for send clock to 1ms is ok, but If I triewd to set less than 1ms I cannot. Can somebody help me the reason? Thanks in advance. MaxT1978
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/14/2023 14:20:05New subject after splitting |
|
1/18/2024 8:14 AM | |
Joined: 12/10/2011 Last visit: 7/10/2024 Posts: 39 Rating:
|
Nobody may help me? Massimo |
3/20/2024 2:06 PM | |
Joined: 12/10/2011 Last visit: 7/10/2024 Posts: 39 Rating:
|
Can somebody help me about it please? Thanks in advance. MAssimo |
Follow us on