9/2/2015 11:13 AM | |
Joined: 4/15/2014 Last visit: 12/4/2023 Posts: 2 Rating: (0) |
Hi! There was a problem while checking communications controller 1200 sm- c module CB1241 protocol MODBUS. The controller itself is in SLAVE mode to the external device it has to read a fault occurs in the system. The program itself looks like and does not issue error. If you attempt to read information from the port of getting «CRC Error» and «Time out error». but I see the port count with him I can not external device .What's the problem until I find out I can not. Yelp is needed. Attachmentpictures.doc (92 Downloads) |
Follow us on