9/23/2020 5:49 AM | |
Joined: 9/2/2020 Last visit: 3/5/2024 Posts: 60 Rating: (0) |
Dear ChristophD I have problem with CF card in a machine. when i put the CF in slot, it is not recognized and 7 segment of controller (SimotionD425) show,s 0--2--0------ 0--2--0------ and repeat this. what happened for CF do you think? Regards ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/23/2020 14:28:51New subject after splitting |
|
9/23/2020 9:38 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
mlfb= order number work the card in a usb card reader? |
9/23/2020 9:51 AM | |
Joined: 9/2/2020 Last visit: 3/5/2024 Posts: 60 Rating: (0) |
Hi Yes it works. |
9/23/2020 10:26 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
and which data is on the card? |
9/23/2020 11:12 AM | |
Joined: 9/2/2020 Last visit: 3/5/2024 Posts: 60 Rating: (0) |
Hi This is content of CF. |
9/23/2020 11:16 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
can you attach the content.txt file here? |
9/23/2020 11:31 AM | |
Joined: 9/2/2020 Last visit: 3/5/2024 Posts: 60 Rating: (0) |
Hi See content.txt file AttachmentCONTENT.TXT (172 Downloads) |
Follow us on