7/18/2019 10:31 PM | |
Posts: 1 Rating: (0) |
Could anyone share a download link for wincc 2008 flexible? There is a project that working on wincc flexible 2008 sp2 and I have to chane a tag address on on screen. I tried to change with sp3 but when I install sp3 on worked pc it tried to delete runtime sp2 licenced. So I do not install sp3. is sp3 usage break the sp2 hmi settings on runtime licences with sp2 if I tried to change hmi program on my pc? I am searcing for download wincc flexible 2008. I have sp1 and sp2 but not first version.. or any other suggestion? thanks. ------------------------------------------------------------------------------------------ |
Last edited by: ibabaoglan at: 07/18/2019 22:33:57Last edited by: Jen_Moderator at: 07/19/2019 07:09:07New subject after splitting Last edited by: ibabaoglan at: 07/19/2019 09:53:51 |
|
7/23/2019 9:48 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello ibabaoglan there is no free download of WinCC flexible older than V2008 SP3 LINK You can try to contact your local Siemens Presales Support for help. -> you can also try to install everything to SP3. Nothing should delete any licenses!! Its because you need the same License for every Version of WinCC flexible 2008 (Servicepack is not essential) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on