1/2/2024 10:06 AM | |
Joined: 6/21/2022 Last visit: 1/8/2024 Posts: 28 Rating: (0) |
Hello How that can be done? I need to change language from german to english in Sinumerik 805 on Bdf Dus 506 lathe. Do I have to rotate start up switch on Sinumerik module in position 2 and then to select Nc Md bits tab in Sinumerik standard UI? Now I see just custom UI,set by manufacturer? Can that bit change cause some problem in default UI or later in work? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/02/2024 11:39:16New subject after splitting |
|
1/2/2024 11:40 AM | |
Joined: 6/19/2017 Last visit: 5/15/2024 Posts: 8062 Rating: (164) |
Closed cause question posted twice. The second thread with the subject Change language in Sinumerik 805 is published within the conference SINUMERIK CNC automation systems. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on