3/28/2024 7:45 AM | |
Joined: 1/21/2013 Last visit: 5/10/2024 Posts: 2765 Rating: (448)
|
Hi Miguel, Writing a JavaScript function to change the screen can be done in several ways. For example, you can use the ChangeScreen method. However, in WinCC Unified, a scheduled task cannot be used to perform a screen change on value change. However, you can use dynamization within your UI to achieve your goals. You need to find an object that is always visible to configure a dynamization for one of its properties. You probably do not want to change its property, so your script should return the default value of the property. But you can use the dynamization to trigger the script you want to run when the tag value changes. Kind regards |
3/28/2024 2:56 PM | |
Joined: 11/7/2022 Last visit: 4/17/2024 Posts: 6 Rating: (0) |
Hi Stefan; Thanks for reply, let me check the link you shared. |
Follow us on