Industry Online Support
Technical Forum
5/28/2008 1:27 PM | |
Joined: 4/24/2006 Last visit: 10/8/2024 Posts: 8745 Rating: (1168) |
Hello guntie, You should do the following: You have made a tag in WinCC flexible (tag_1), go to properties of the mentioned tag. Then you go to Events -> change value Now you can choose function: ActivateScreenByNumber. And you select tag_1 for Screen number. So if you put 11 in tag_1, the screen with screennumber 11 will be activated. Here you find more information in link: http://support.automation.siemens.com/WW/view/en/25011172 http://support.automation.siemens.com/WW/view/en/24372775 Best regards, Wizard |
Follow us on